adccommunitymod (AutomationDirect) asked a question.

Logging for Dummies - EA9

Created Date: October 24,2017

Created By: jerrygontarz

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Howdy, Though long experienced with the C-More Micro, I just started a project with the C-More EA9. I want to write a number of tags to a USB drive, but can't figure it out. I can write an alarm.txt file that has some tags all concatenated together, but that's not what I am after. Ideally, I'd specify a fragment of a filename "Log X " - the log file would presumably auto increment the number appended to the filename and it would contain: Start Date: Oct 24 2017 Start Time:12:47 PM Equipment Serial Number: X56798732 Asset Number: 372676XC Product Name: Widgets Operator: FD Total Process Duration: 12:30 Minutes Set Speed: 18 Actual Speed 1: 17.88 Actual Speed 2: 18.02 Actual Speed 3: 17.97 Actual Speed 4: 17.88 End Date: Oct 24 2017 End Time: 12:59 PM Getting the data into tags is not an issue, getting them written to a file has me completely perplexed. Is this even possible? Thanks Jerry


  • adccommunitymod (AutomationDirect)

    Created Date: October 24,2017

    Created by: jerrygontarz

    Howdy,

    Though long experienced with the C-More Micro, I just started a project with the C-More EA9. I want to write a number of tags to a USB drive, but can't figure it out. I can write an alarm.txt file that has some tags all concatenated together, but that's not what I am after. Ideally, I'd specify a fragment of a filename "Log X " - the log file would presumably auto increment the number appended to the filename and it would contain:

    Start Date: Oct 24 2017

    Start Time:12:47 PM

    Equipment Serial Number: X56798732

    Asset Number: 372676XC

    Product Name: Widgets

    Operator: FD

    Total Process Duration: 12:30 Minutes

    Set Speed: 18

    Actual Speed 1: 17.88

    Actual Speed 2: 18.02

    Actual Speed 3: 17.97

    Actual Speed 4: 17.88

    End Date: Oct 24 2017

    End Time: 12:59 PM

    Getting the data into tags is not an issue, getting them written to a file has me completely perplexed. Is this even possible?

    Thanks

    Jerry

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: October 28,2017

    Created by: mwdkmpr

    Use the event manager.

  • adccommunitymod (AutomationDirect)

    Created Date: June 28,2018

    Created by: Dumarest

    I don't see any way in the Event Manager to write to a file!

  • adccommunitymod (AutomationDirect)

    Created Date: June 29,2018

    Created by: sii

    Toward the bottom of the Add Event dialog box is a checkbox labeled 'save file to SD1 '. I 've never used it so I'm not sure beyond that but that should get you started.

  • adccommunitymod (AutomationDirect)

    Created Date: July 05,2018

    Created by: Orion HE

    I don't believe the C-more allows you to do anything special with filename. It's very limited. We use a Do-more to write to a file and email it daily. Let us know if you find a solution. I value knowing different ways to solve a problem.

  • adccommunitymod (AutomationDirect)

    Created Date: July 08,2018

    Created by: Tom@Pton

    I have used C-more event manager to email me a text file every night. It includes graph information averaged and recorded every 5 seconds for, 2 temperatures sensors, 3 rpm counters, 1 HZ setting for a VFD and 4 motor amperages. Works well.