adccommunitymod (AutomationDirect) asked a question.
Converting C-More protocol from Do-More to Do-More Full Memory
Created Date: October 18,2017
Created By: Frontier
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
C-More 6.31 enabled full access to the Do-More memory range. If I change the PLC protocol from the original "Built-in memory only " option to the "Full Memory " option, it says all tags will be set to 'Internal ', meaning they will lose any reference to the original PLC addresses. Is there a way to avoid this? It would be kind of a drag to have to rebuild the entire HMI project.
Created Date: October 18,2017
Created by: Frontier
C-More 6.31 enabled full access to the Do-More memory range. If I change the PLC protocol from the original "Built-in memory only " option to the "Full Memory " option, it says all tags will be set to 'Internal ', meaning they will lose any reference to the original PLC addresses.
Is there a way to avoid this? It would be kind of a drag to have to rebuild the entire HMI project.
Created Date: October 18,2017
Created by: BobT65
I think your only other option is to add another device to the C-more using the new driver. Then you can use both drivers at the same time with the same PLC. Leave all of the original driver tags as is and create new tags with the new driver.
I expect the conversion in software quite difficult.
There may be something you can do with exporting and importing.
Created Date: October 18,2017
Created by: BobO
I'm not familiar with C-more, but if it is possible to have more than one driver, I would definitely leave everything that works as is. Just add new stuff on the other driver, and only things which you can't access from the original driver.
The original Do-more driver is built on the programming protocol that DmD uses. It's fast. The C-more team could have used it to access everything, but there are a hefty pile of complexities associated with the memory map being infinitely flexible, so they chose to keep their access limited. We added the new symbolic protocol to simplify access to everything else, but because all tag references have to be converted from a symbol name to a physical address in the PLC, it's much slower than the native programming interface.
Created Date: October 19,2017
Created by: jackson
Topic CM041 of the C-more Programming software help file confirms what both 'Bobs ' above just said: "Both drivers may be used simultaneously. Use the Built-in memory driver for all of the default memory addresses and use a Symbolic Addressing driver for any user-added memory. The two drivers can even co-exist for one PLC in the C-more project. "