adccommunitymod (AutomationDirect) asked a question.
Created Date: August 19,2017
Created By: skyfox
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Hello All, I get a message on C-more panel every time I Boot-UP asking click ignore to continue without data logging. (SD Cards not detected) 1. I am not asking my program to log anything. (Not Tags, Not Messages (from MSG DB) , No Alarms, and events. In fact I have no Alarms or events configured as of yet. 2. In the panel settings, under panel manager "LOG " option is unchecked. This is a brand new panel. In fact I am working with two new panels but not identical programs. Only one panel is doing this. And then while the HMI program is running....it intermittently flashes the Message "RTE-002 Log Message " failed ". And also see a message that it is unable to access log text file (don't remember the message exactly) What is causing this? How do I get rid of it? Thanks!
Created Date: August 19,2017
Created by: skyfox
Hello All,
I get a message on C-more panel every time I Boot-UP asking click ignore to continue without data logging. (SD Cards not detected)
1. I am not asking my program to log anything. (Not Tags, Not Messages (from MSG DB) , No Alarms, and events. In fact I have no Alarms or events configured as of yet.
2. In the panel settings, under panel manager "LOG " option is unchecked.
This is a brand new panel. In fact I am working with two new panels but not identical programs. Only one panel is doing this.
And then while the HMI program is running....it intermittently flashes the Message "RTE-002 Log Message " failed ". And also see a message that it is unable to access log text file (don't remember the message exactly) What is causing this? How do I get rid of it?
Thanks!
Created Date: August 21,2017
Created by: HMI Eng
Check all of your Line Trend Objects and make sure you have not checked Save Log Data
Also, put an SD card in the slot for a little while, pull it and look at the log files. The name of the files should point you to the source.