adccommunitymod (AutomationDirect) asked a question.
C-More Micro Software Version 4.10
Created Date: April 28,2017
Created By: bcarlton
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
After creating a project I can re-open just fine from within the software. But I can't see the .mgp files (using Windows File Explorer) I created in the 'Project ' folder. I do see a few default files which I also see when opening from within the software. (Windows 10 Home 64 bit)
Created Date: April 28,2017
Created by: bcarlton
After creating a project I can re-open just fine from within the software. But I can't see the .mgp files (using Windows File Explorer) I created in the 'Project ' folder. I do see a few default files which I also see when opening from within the software. (Windows 10 Home 64 bit)
Created Date: April 29,2017
Created by: Ridgeline Mach
Created a test project, and found the same issue. Same operating system; Windows 10 Home 64-bit. Weird.
Created Date: April 29,2017
Created by: bcarlton
Thanks for verifying that I'm not totally insane at least.
Created Date: April 29,2017
Created by: kewakl
I haven't taken the swim in the Windows 10 koolaid yet, so this is a shot in the dark...
Does Win10 do the 'virtual store ' thing the Win7 did? and can you turn it off.
I have a laptop that the original user did not disable the virtual store and I have to hunt stuff all of the time.
https://support.microsoft.com/en-us/...r-in-windows-7
Scenario 2: You cannot find the file or the folder that you just created
When you use an application for which virtualization is enabled, you create data files in virtualizable locations of the file system. When you use another application or Windows Explorer to access these newly created files, you cannot find them. For example, if you save a file in a photo editing application in the %programfiles%, %systemroot%, %systemdrive%, or %programdata% folders, you cannot locate this file.
.
.
.
Scenario 2
To resolve this issue, use one of the following methods:
Click the Compatibility Files button that appears on the Explorer bar to view virtualized files in the folder. The Compatibility Files button appears only if there are virtualized files in the folder.
Look in the C:\Users\ User_name \AppData\Local\VirtualStore folder to locate files and folders.
Save your application's data in a folder under your user profile.
EDIT: this post was composed on a Windows XPSP3 laptop :p
Created Date: April 29,2017
Created by: bcarlton
Look in the C:\Users\ User_name \AppData\Local\VirtualStore folder to locate files and folders.
That's where they were. Why not store them in the standard place?
I cut from 'virtualstore ' and pasted them in the standard place. It could open them from there but, on saving, it stored them in 'virtualstore '. This happened even if I chose 'Run As Administrator '.
Re-installed application - still doing it.
Created Date: April 29,2017
Created by: kewakl
As I understand it, Virtual Store is M$'s way to force APPLICATIONS programmers to stop writing to application's folders.
If an application does NOT conform to the Vista/Win7++ way to store APPLICATION DATA, programs, datafiles... that data will be written to a virtual store that GHOSTS/MIMICS the application's folders.
You may have to TAKE OWNERSHIP of the PROJECTS folder.
I have Win7 (on this PC) so (for me) it would be:
Navigate to C:\Program Files (x86)\AutomationDirect\C-more micro\Project
Right Click on the Project folder
Properties
Security tab
click the Edit... button
in the ' Group or user names ' list select your user profile Users( _username_ \ _groupname_ ) where in my case this would read Users(Me-PC\Users)
Award yourself all the required permissions in the Allow column
click Apply/OK as desired.
From Windows version to Windows version the names/descriptions may have changed, but the intent should be similar.
I do not know if you need to restart CmoreMicro or not.
Created Date: April 29,2017
Created by: bcarlton
Thanks, your last suggestion may have done the trick.
Created Date: April 29,2017
Created by: kewakl
Glad to return some help!