adccommunitymod (AutomationDirect) asked a question.

issue when using app and view over IE

Created Date: August 05,2016

Created By: Ajb86

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

We have an application where we have a tablet setup with the Cmore app and we have a pc setup to remote view the HMI screen when both are running we have a lot of lag and even drops out the application, the view port is set at default (11102) are we loading this up by running both at the same time. When I disconnect the Wifi For tablet the remote view on the pc works 100% does anyone run a similar setup and if so do you have any issues?


  • adccommunitymod (AutomationDirect)

    Created Date: August 05,2016

    Created by: Ajb86

    We have an application where we have a tablet setup with the Cmore app and we have a pc setup to remote view the HMI screen when both are running we have a lot of lag and even drops out the application, the view port is set at default (11102) are we loading this up by running both at the same time.

    When I disconnect the Wifi For tablet the remote view on the pc works 100%

    does anyone run a similar setup and if so do you have any issues?

    Expand Post