adccommunitymod (AutomationDirect) asked a question.

Point of View with Click ethernet

Created Date: July 06,2016

Created By: daakers

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I'm wanting to use Point Of View with a Click C0-10DD2E-D plc. Via the ethernet port but not having much luck. Will this work? If so are there any videos or help pages for this? Also while just messing around with it here at the shop I was able to connect POV to port 2 as per the video, but I can not seem to get C1 in the Click to work with a PB on POV. I have the address in POV as 1X:16385? I can monitor Y1 at 0X:8193?? Been so long since I done any Modbus it's going to be something I doing wrong.


  • adccommunitymod (AutomationDirect)

    Created Date: July 06,2016

    Created by: daakers

    I'm wanting to use Point Of View with a Click C0-10DD2E-D plc. Via the ethernet port but not having much luck. Will this work? If so are there any videos or help pages for this?

    Also while just messing around with it here at the shop I was able to connect POV to port 2 as per the video, but I can not seem to get C1 in the Click to work with a PB on POV. I have the address in POV as 1X:16385? I can monitor Y1 at 0X:8193?? Been so long since I done any Modbus it's going to be something I doing wrong.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: July 06,2016

    Created by: daakers

    Ok I knew it was me LOL. I'm starting to remember I hate getting old and working 2 shifts! I got it the C's should also be OX:16385 LOL