adccommunitymod (AutomationDirect) asked a question.
Created Date: June 23,2016
Created By: kewakl
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I have 13 panels (all EA7) on two separate lines and on separate data networks. Several of these screens do the occasion Black/White screen crash. No permanent fix has been found First line: PanelName Model OD(Date) Runtime System Screensaver Black/ Hardware BOOT Hardware? Screen InUse WhiteScreen (No description) DataControl_1 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.08 2000 0000-0000-0000-0020 DataControl_2 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.03 2000 0000-0000-0000-0008 Conveyor EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.03 2000 TT EA7-T8 10-12-2012 2.78 2.78 N N 1400N REV.05 2000 0000-0000-0000-0018 CAPESR EA7-T15 10-12-2012 2.77 2.77 N N 1200 REV.01 2000 DCL EA7-T15 05-07-2010 2.72 2.72 Y Y 1200 REV.01 2000 SORTEXIT EA7-T8 03-09-2012 2.78 2.78 N N 1400N REV.05 2000 0000-0000-0000-0018 Second line: PanelName Model OD(Date) Runtime System Screensaver Black/ Hardware BOOT Hardware? Screen InUse WhiteScreen (No description) Master EA7-T15 10-12-2012 2.78 2.78 Y Y 1200N REV.04 2000 0000-0000-0000-0008 StaC11 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.03 2000 0000-0000-0000-0008 StaC12 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200 REV.00 2000 StaC13 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.03 2000 0000-0000-0000-0008 StaC14 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.07 2000 0000-0000-0000-0020 StaC15 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.07 2000 0000-0000-0000-0020 I was nearly finished gathering this data when I considered that Hardware and BootLoader could be of some importance. If it is, please reply to this thread. I will also check to verify dedicated power supplies on each panel. One thing to note: On StaC11 - StaC15, If the screensaver is active when I request a screen change, the screen blinks ON and then back off. I send multiple requests and usually the screen comes on and stays on. ?? (I need to double-check the OSDate/Runtime and SystemScreen info above.) If it is important, I can get the pertinent info on the PAC cpu's in the lines.
Created Date: June 23,2016
Created by: kewakl
I have 13 panels (all EA7) on two separate lines and on separate data networks.
Several of these screens do the occasion Black/White screen crash. No permanent fix has been found
First line:
PanelName Model OD(Date) Runtime System Screensaver Black/ Hardware BOOT Hardware?
Screen InUse WhiteScreen (No description)
DataControl_1 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.08 2000 0000-0000-0000-0020
DataControl_2 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.03 2000 0000-0000-0000-0008
Conveyor EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.03 2000
TT EA7-T8 10-12-2012 2.78 2.78 N N 1400N REV.05 2000 0000-0000-0000-0018
CAPESR EA7-T15 10-12-2012 2.77 2.77 N N 1200 REV.01 2000
DCL EA7-T15 05-07-2010 2.72 2.72 Y Y 1200 REV.01 2000
SORTEXIT EA7-T8 03-09-2012 2.78 2.78 N N 1400N REV.05 2000 0000-0000-0000-0018
Second line:
PanelName Model OD(Date) Runtime System Screensaver Black/ Hardware BOOT Hardware?
Screen InUse WhiteScreen (No description)
Master EA7-T15 10-12-2012 2.78 2.78 Y Y 1200N REV.04 2000 0000-0000-0000-0008
StaC11 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.03 2000 0000-0000-0000-0008
StaC12 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200 REV.00 2000
StaC13 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.03 2000 0000-0000-0000-0008
StaC14 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.07 2000 0000-0000-0000-0020
StaC15 EA7-T12 10-12-2012 2.78 2.78 Y Y 1200N REV.07 2000 0000-0000-0000-0020
I was nearly finished gathering this data when I considered that Hardware and BootLoader could be of some importance.
If it is, please reply to this thread.
I will also check to verify dedicated power supplies on each panel.
One thing to note: On StaC11 - StaC15, If the screensaver is active when I request a screen change, the screen blinks ON and then back off.
I send multiple requests and usually the screen comes on and stays on. ??
(I need to double-check the OSDate/Runtime and SystemScreen info above.)
If it is important, I can get the pertinent info on the PAC cpu's in the lines.
Created Date: June 23,2016
Created by: plcnut
I do not remember the details, but I did find an issue at one time where the "start screensaver " appeared to overlay a screensaver on top of a screensaver. In other words, if the screen had been inactive for long enough to have the screensaver triggered 3 times, then I would have to tap the screen 3 times to get the screensaver to release the screen. This project was using the PLC to turn the screensaver on.
Created Date: June 23,2016
Created by: kewakl
I do not remember the details, but I did find an issue at one time where the "start screensaver " appeared to overlay a screensaver on top of a screensaver. In other words, if the screen had been inactive for long enough to have the screensaver triggered 3 times, then I would have to tap the screen 3 times to get the screensaver to release the screen. This project was using the PLC to turn the screensaver on.
Interesting, but I am letting the cmore timeout feature do this for me, maybe it is timing out multiple times.... Maybe this is causing the panel to crash.
I am trying to WAKE the screen.
I let it sleep until either a touch or a request from the master PAC. When the operator scans a barcode tag below the screen (in preparation to an automated setup) the screen should wake and GOTOSCRN should call the correct screen. It does wake, but the sleeps again. So, the multiple WAKE (GOTOSCRN) requests.
The wireless barcode scanner is connected to the RJ12 Serial port of the MASTER PAC. The master's task is to coordinate all DATA from the 5 stations to a DATAWORX install. So Master tells the stations ' PAC to tell the screen to wake.
Sorry If I led you to think that I was putting it to sleep.
Created Date: June 23,2016
Created by: plcnut
You did not lead me to believe anything. I was only hoping that some of my experiences may help to put together a common denominator. I replaced the EA7 that was giving trouble with an EA9 and did away with the PLC calling the screensaver at the same time, so have not done any further testing.
Created Date: June 24,2016
Created by: plcnut
My panel with issues also included item(s) that were outside the view-able area.
(I use a text entry object with a USB bar-code scanner as an input and leave it outside the viewing area for aesthetics).
----------------------------------------------------------------------------------------------------
This post is in regards to this same issue that is also being discussed in another forum
Created Date: June 24,2016
Created by: Do-more PE
Off screen stuff is handled just like on screen stuff with the exception of you just can't see it.
Created Date: June 27,2016
Created by: a agnone
Only time I experienced the white screen when I was using the 120v adapter to power the panel. I since then do not use them. I power up from a separate 24v power supply, other then want I use for the rest of the machine. I have not had any issues. I think they may have fixed that problem, but I still use a separate power supply for my HMI. Actually I only use the separate power supply if I am going to have lots of relays or a contactor. I know, cost more but it has been working for me.
Created Date: June 30,2016
Created by: kewakl
Only time I experienced the white screen when I was using the 120v adapter to power the panel. I since then do not use them. I power up from a separate 24v power supply, other then want I use for the rest of the machine. I have not had any issues. I think they may have fixed that problem, but I still use a separate power supply for my HMI. Actually I only use the separate power supply if I am going to have lots of relays or a contactor. I know, cost more but it has been working for me.
Interesting, I installed those EA_AC pods because of AD tech recommendation to try to stop the black/white screens.
Historically, I have NOT installed dedicated power supplies (until AD tech recommendation for this issue) except in cases with contactors/relays, etc.
Created Date: April 21,2017
Created by: kewakl
In the list in OP, I have removed all screensavers in the section labeled 'second line: '
I did this in mid January. So far, I have not logged any more whitescreen crashes on those panels.
Thanks to any / all who have contributed to resolving this -- in this and other threads / forums.
Created Date: March 24,2018
Created by: kewakl
As far as this weekend, I have not seen any whitescreen crashes on the panels that I removed the screensavers.
(prompted to update this thread from pbw's query https://forum.automationdirect.com/forum/operator-interface/112179-c-more-freeze )