adccommunitymod (AutomationDirect) asked a question.

CLICK to EA3-T6CL

Created Date: February 12,2016

Created By: cmacdonald

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Hi All, I am wondering if there is a way to activate a discrete tag momentarily from a recipe button? Either that or is there a way to overlay two buttons and have them both work? What I am looking to do is load a set of parameters and operate a start button with one push. I appreciate your help, Cam


  • adccommunitymod (AutomationDirect)

    Created Date: February 12,2016

    Created by: bcarlton

    Set one of your parameters in your recipe to a TRUE state in all the recipes. When the program notices that location change to TRUE it triggers the start then sets the location false.

  • adccommunitymod (AutomationDirect)

    Created Date: February 16,2016

    Created by: cmacdonald

    CLICK to EA3-T6CL

    Hi bcarlton,

    Thanks for your reply, but I'm not getting it. I don't get an option for a logic 'true ' I simply get an option for a constant 1 or 0 which sets the bit which has to be cleared. Is this an internal tag that I'm manipulating?

    I am also having an issue using a momentary setting for a pushbutton that the PLC does not respond to for no obvious reason, but not every time. Sometimes it works when I reload the same program.

    Thanks for your help,

    Cam

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: February 12,2016

    Created by: cmacdonald

    Hi All,

    I am wondering if there is a way to activate a discrete tag momentarily from a recipe button? Either that or is there a way to overlay two buttons and have them both work? What I am looking to do is load a set of parameters and operate a start button with one push.

    I appreciate your help,

    Cam

    Expand Post