adccommunitymod (AutomationDirect) asked a question.

PLC-028 Error code

Created Date: May 26,2015

Created By: omaragomez

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Hello everyone. I'm using a DL-6 AR and Cmore EA9-T6CL. I'm communicating thru serial using the K-Sequence protocol. The PLC is being used for monitoring water tanks. It's been installed and running for a year. Recently I 've been getting error codes "PLC-028 " and it has lead to making the PLC Freeze with closed relays. The only way I have gotten it to unfreeze was by shutting down power and then back up. I never had that problem before. Any solutions? Thanks in advanced.


  • adccommunitymod (AutomationDirect)

    Created Date: June 03,2015

    Created by: nmatthews22

    Same issue!

    I have the same issue with my application. I'm using a EA9-T6CL-R with D0-06DD2. The message appeared randomly but everything seems to function normally.

    Call Automation Direct today and waiting to hear back from them.

  • adccommunitymod (AutomationDirect)

    Created Date: May 26,2015

    Created by: omaragomez

    Hello everyone. I'm using a DL-6 AR and Cmore EA9-T6CL. I'm communicating thru serial using the K-Sequence protocol. The PLC is being used for monitoring water tanks. It's been installed and running for a year. Recently I 've been getting error codes "PLC-028 " and it has lead to making the PLC Freeze with closed relays. The only way I have gotten it to unfreeze was by shutting down power and then back up. I never had that problem before. Any solutions?

    Thanks in advanced.

    Expand Post
  • AndrAske (Customer)

    I had the same issue as nmatthews22. I had to increase the Baud Rate from 9600 to 19200. There is useful information on how to do this in the Help section on the C-more Programing Software, expand PLCs Setup and choose what PLC you are using.

  • Donetop (Customer)

    Please I have this issues too plc 028 failed for a DL260 cpu. This results in a thing pressed on the HMI has no change or effect on the panel but the beeps you hear as you press the HMI.

     

    Plea wwhat is the possible solution