adccommunitymod (AutomationDirect) asked a question.
Created Date: February 12,2014
Created By: IntelliMation
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I am using a recipe to load info to a DL06. 1 Alpha, 2 Digital, and 27 BCDs. I am using internal tags for storing the info for each of 49 recipes. I have a "Load " button on each recipe screen that loads the info for that recipe to the DL06. So the DL06 only has the data for the recipe that has been loaded and is running. The problem is that I can't pull all of this info out of the C-more by saving the recipe to a USB. I only get the tag names if I remember correctly. I went the tag route so that I could make the UI look the same as the operators are used to for another project. Anybody have any thoughts on being able to retrieve the data from the C-more. I need to update some older C-mores with the latest program and I will have to manually copy all of the info from all of the used recipes so that I can then manually reload it after the update (PITA).
Created Date: July 02,2015
Created by: IntelliMation
Recipes and USB
Anyone have any thoughts.
Created Date: July 02,2015
Created by: HMI Eng
I would recommend using the Call Recipe object with a Recipe Sheet, but as you said that may not have the same look your operators are used to.
Created Date: February 12,2014
Created by: IntelliMation
I am using a recipe to load info to a DL06. 1 Alpha, 2 Digital, and 27 BCDs. I am using internal tags for storing the info for each of 49 recipes. I have a "Load " button on each recipe screen that loads the info for that recipe to the DL06. So the DL06 only has the data for the recipe that has been loaded and is running. The problem is that I can't pull all of this info out of the C-more by saving the recipe to a USB. I only get the tag names if I remember correctly. I went the tag route so that I could make the UI look the same as the operators are used to for another project. Anybody have any thoughts on being able to retrieve the data from the C-more. I need to update some older C-mores with the latest program and I will have to manually copy all of the info from all of the used recipes so that I can then manually reload it after the update (PITA).