adccommunitymod (AutomationDirect) asked a question.
using a 15" Cmore with DoMore
Created Date: January 07,2014
Created By: jparker
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Is the only way to use the EA7-T15C with a DoMore is thru ethernet? Or am I missing something? Thanks for any input
Created Date: January 07,2014
Created by: scott.lawrence
you can set the serial port up in s/w
I haven't tried this, b/c we put everything on ethernet :)
Created Date: January 07,2014
Created by: jwbaker3
The CPU's have a RS232 RJ12 connector, and the C-more has a protocol for Do More serial. Click the "SETUP " in the Cmore software, select the panel type from the drop down menu, under COM Port (on the left side) click on the "DEV001 " this will bring up the protocol selection, click on the "PLC Protocol " and the "Automation Direct Do More serial " will show up on the drop down menu. Use this (EA-2CBL) cable.
JW
Created Date: January 07,2014
Created by: jparker
Is the only way to use the EA7-T15C with a DoMore is thru ethernet? Or am I missing something?
Thanks for any input