adccommunitymod (AutomationDirect) asked a question.

C-More slow to Update screen

Created Date: November 11,2013

Created By: daturner

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Our latest project has the newest version of C-More v2.78. It is linked to a DL205 (CPU is a 260) with a slave that is also a DL205 base. These are linked to a Red Lion CPU unit that has 10 of their modules on a rack. This is an extruder set up. We have several machines set up like this BUT this is the only one that the C-More screen is extremely slow to update, ( five seconds or longer). The only thing that is different than all of the other machines is the fact that the version is 2.78 for the C-more AND we are running a slave. And we use the #2 port on the 260 to talk to a Clinton sparker that has to communicate via the RS 232 serial link. Everything else is communicating via Ethernet. Any ideas? We have searched for the cause for hours.


  • adccommunitymod (AutomationDirect)

    Created Date: December 02,2013

    Created by: daturner

    Found the problem...finally

    Data logging to the chart screen was causing the slow down. Which basically means we can't run charts 24/7 to track issues...but what the heck.

  • adccommunitymod (AutomationDirect)

    Created Date: December 02,2013

    Created by: OpZed

    C-more is connected to Port1 at 9600 baud?

  • adccommunitymod (AutomationDirect)

    Created Date: December 03,2013

    Created by: daturner

    C-More issues

    We use Ethernet for the C-More and 205 PLC rack and other units.

  • adccommunitymod (AutomationDirect)

    Created Date: December 07,2013

    Created by: LWgreys

    Sounds more like an overhead problem in the PLC.

    Are you using any loops in the plc program?

    Have you checked the plc scan times?

  • adccommunitymod (AutomationDirect)

    Created Date: November 11,2013

    Created by: daturner

    Our latest project has the newest version of C-More v2.78.

    It is linked to a DL205 (CPU is a 260) with a slave that is also a DL205 base.

    These are linked to a Red Lion CPU unit that has 10 of their modules on a rack. This is an extruder set up.

    We have several machines set up like this BUT this is the only one that the C-More screen is extremely slow to update, ( five seconds or longer).

    The only thing that is different than all of the other machines is the fact that the version is 2.78 for the C-more AND we are running a slave. And we use the #2 port on the 260 to talk to a Clinton sparker that has to communicate via the RS 232 serial link.

    Everything else is communicating via Ethernet.

    Any ideas? We have searched for the cause for hours.

    Expand Post