adccommunitymod (AutomationDirect) asked a question.

Using outs more the one place

Created Date: March 21,2013

Created By: vf816

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I am writing a manual mode to a program I am trying to do using a sub routine.I have inputs turning on the outputs in the main program when in auto mode and I want to have buttons on a Cmore panel turn on the same outputs in manual mode.Is there any problem with trying to do it this way. I do get the warnings but no errors when doing the program check. Any thoughts?


  • adccommunitymod (AutomationDirect)

    Created Date: March 22,2013

    Created by: bcarlton

    A better way would be to end each of you current rungs with a unique C bit.

    In the Auto section you would have a rung ending in Widget_On_Auto

    In your manual section have the equivalent rung ending in Widget_On_Manual

    Then finally have a section where the outputs are actually controlled. It would have a rung with

    Widget_On_Auto

    in parallel with

    Widget_On_Manual --- leading to the real output Y_Something - Widget On

    There is another method called OROUT available on some CPUs but I find it to be more confusing than helpful.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: March 22,2013

    Created by: franji1

    I did an app where you would put the system in auto mode vs. manual mode. The manual mode bits were controlled by the HMI. However, we did not want the HMI to be able to manipulate the actual output when in Auto mode. The logic for many of the "turn something on " looked like

    ManualOnA AutoMode A

    ---] /

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: March 22,2013

    Created by: vf816

    This is what I have now

    bcarlton

    This is the start of a rough draft I have.

    I am not sure I understand you correctly

    Could you add what you are saying at the end of what I have?

    Thanks

  • adccommunitymod (AutomationDirect)

    Created Date: March 22,2013

    Created by: vf816

    franji1

    Hey thanks I was just asking for that now I remember?

    Thanks again to all that help this form rocks.It is a great place to learn

    I think I am officially an Automation Direct JUNKIE:D

  • adccommunitymod (AutomationDirect)

    Created Date: March 21,2013

    Created by: vf816

    I am writing a manual mode to a program I am trying to do using a sub routine.I have inputs turning on the outputs in the main program when in auto mode and I want to have buttons on a Cmore panel turn on the same outputs in manual mode.Is there any problem with trying to do it this way.

    I do get the warnings but no errors when doing the program check.

    Any thoughts?

    Expand Post