adccommunitymod (AutomationDirect) asked a question.
Remote Access question
Created Date: March 06,2013
Created By: mb100
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Why can i remote access a cmore panel using the cmore iphone app but not with the built in cmore client. I can remotely reach the cmore web server screen and download the client but the client can not remote access. I would assume that if port 11102 was being blocked the iphone ap would not work either. It may have something to due with the VPN setup since I have to manually enter the webserver port (:8080) to reach the cmore web server.
Created Date: March 06,2013
Created by: mb100
Figured it out. Instead of using the automatically assigned name from the client which uses the screens actual IP. EA-CON_IP= I had to rename the client EA-CON_IP= where remote.vpndnsname.org is the VPN DNS
Created Date: March 06,2013
Created by: mb100
Why can i remote access a cmore panel using the cmore iphone app but not with the built in cmore client. I can remotely reach the cmore web server screen and download the client but the client can not remote access. I would assume that if port 11102 was being blocked the iphone ap would not work either. It may have something to due with the VPN setup since I have to manually enter the webserver port (:8080) to reach the cmore web server.