adccommunitymod (AutomationDirect) asked a question.

Cmore Micro display binary instead of BCD

Created Date: October 23,2012

Created By: crod

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

On Cmore Micro 6 " HMI. Trying to display status of 64 discrete inputs read from Vmemory, 40400, 40401, 40402, 40403. Would like to display 0/1 for OFF/ON status in 4 bit nibbles, as in following example. 40400 0101 1001 0110 1100 40401 1011 0110 1010 0011 Is this possible? BCD numeric display is confusing. 64 Discretes maxes out dynamic object use when outputs are added.


  • adccommunitymod (AutomationDirect)

    Created Date: October 23,2012

    Created by: Tubecut

    What PLC are you using?

    I don't see how you can do that with just HMI programming.

    I think you can do it using PLC code to cycle through the V memory value(s).

  • adccommunitymod (AutomationDirect)

    Created Date: October 23,2012

    Created by: franji1

    I think he's wondering if there is a "display mode " or "display format " in the HMI to display binary values.

    For example, the new Do-more Designer's Data View (DirectSOFT equivalent for Do-more) has a "binary format " for numeric values. When it displays the value, instead of displaying a stream of 1's and 0's, it splits them up by "hex digit " with underscores, e.g. the value 0xF00D would display as

    1111_0000_0000_1101

    Do-more uses under scores to separate the the "hex digits ", he showed spaces in his example.

    So, is there a binary display format in Cmore Micro that can do this?

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: October 23,2012

    Created by: crod

    DL205, 250-1 CPU but want to avoid PLC code.

    franji1 is correct, just wondering if the HMI has different a display method.

    Hex or Octal would be OK. It's difficult or impossible to distinguish individual bits in BCD display.

  • adccommunitymod (AutomationDirect)

    Created Date: October 23,2012

    Created by: Tinker

    DL205, 250-1 CPU but want to avoid PLC code.

    franji1 is correct, just wondering if the HMI has different a display method.

    Hex or Octal would be OK. It's difficult or impossible to distinguish individual bits in BCD display.

    Oddly enough it almost does, the radio button object can display the bits of memory location, while the radio button only alows one to select one bit, it will display all the bits that are set if they are set by something else. However there are a couple of problems, one fatal, the other an inconvinence. The fatal problem is that is the radio button object will write to the register, so if anyone touches it your data changes, the other problem is that, in the horizontal orientationthe least significant bit is on the left, maybe not a huge problem, but I'd expect to see the LSB on the right.

    I think that being able to display bits can be very usefull for some trouble shooting and status indication apllications, and since the code is allready there all they'd have to do make a bit dispaly object add a "readonly " check box that disables the write register code in the radio button object, but I don't expect that to ever happen, certainly not on a "Micro "

    On a full C-More (not micro) one could password protect a radaio button which could prevent unintentional modification, but it would not be as clean as a readonly dispaly.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: October 23,2012

    Created by: crod

    On Cmore Micro 6 " HMI.

    Trying to display status of 64 discrete inputs read from Vmemory, 40400, 40401, 40402, 40403.

    Would like to display 0/1 for OFF/ON status in 4 bit nibbles, as in following example.

    40400 0101 1001 0110 1100

    40401 1011 0110 1010 0011

    Is this possible?

    BCD numeric display is confusing.

    64 Discretes maxes out dynamic object use when outputs are added.

    Expand Post