adccommunitymod (AutomationDirect) asked a question.

Program SLC5/03 through C-More - possible?

Created Date: July 09,2012

Created By: rguimond

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I have a 6 " C-more communicating with a SLC 5/03 over DH-485. C-More also has its Ethernet port connected to a wireless bridge so I can remotely view it. Is it possible to use the C-More as a bridge between Ethernet and DH-485? I'm guessing there would have to be an EDS file for the C-More so RSLinx can see it, as well as a software setting )port forwarding) within the C-More.


  • adccommunitymod (AutomationDirect)

    Created Date: July 09,2012

    Created by: Do-more PE

    Not currently. It is a feature that is asked for quite often, but there is a lot of work that makes it quite difficult to do.

  • adccommunitymod (AutomationDirect)

    Created Date: July 09,2012

    Created by: rguimond

    I have a 6 " C-more communicating with a SLC 5/03 over DH-485. C-More also has its Ethernet port connected to a wireless bridge so I can remotely view it. Is it possible to use the C-More as a bridge between Ethernet and DH-485? I'm guessing there would have to be an EDS file for the C-More so RSLinx can see it, as well as a software setting )port forwarding) within the C-More.

    Expand Post