adccommunitymod (AutomationDirect) asked a question.

C-more and USB drives

Created Date: April 30,2012

Created By: CribbBc

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I'm trying to use a usb drive to log some data, but the panel doesn't seem to recognize the drive. When the panel boots up it says it's "Detecting USB for logging data ", but never does. Also, if I go into the setup screens to back up or restore from the USB drive it is never recongized there. Are there some kind of size, manufacturer, USB 1/2/3 or file system limitations on valid USB sticks? The panel is a EA7-T6CL, the USB drive is an 8GB Lexar.


  • adccommunitymod (AutomationDirect)

    Created Date: May 01,2012

    Created by: HMI Eng

    Some USB Pen Drives just do not work with C-more. Make sure you have there latest Firmware version in the panel. Format the USB pen Drive as FAT16.

    I have seen pen drives from the same manufacturer but a different chip set where one works and the other does not.

    Frustrating I know.

    8Gb should be no problem.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: April 30,2012

    Created by: CribbBc

    I'm trying to use a usb drive to log some data, but the panel doesn't seem to recognize the drive. When the panel boots up it says it's "Detecting USB for logging data ", but never does. Also, if I go into the setup screens to back up or restore from the USB drive it is never recongized there. Are there some kind of size, manufacturer, USB 1/2/3 or file system limitations on valid USB sticks?

    The panel is a EA7-T6CL, the USB drive is an 8GB Lexar.

    Expand Post