adccommunitymod (AutomationDirect) asked a question.
Recipe Object can load but not save recipe
Created Date: February 22,2012
Created By: jgargel
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I am using the Recipe object to load recipes, but there is no similar object to save the tag values to existing recipes. I know i can use the Call Recipe object to do this, but that is less desirable. I have created graphical screens to change the recipe tag values and would like to save them to the current recipe without using the cumbersome Call Recipe object. Any way to do this? Can this be added as a feature request?
Created Date: February 22,2012
Created by: Do-more PE
Currently this function is not available. I have asked for it to be implemented at some point in the future, but I do not have a timetable as to when that might happen.
Created Date: February 22,2012
Created by: bcarlton
i haven't used recipes from the CMore (we implement them totally within the PLC) so this may be off but recipes can have tags within the PLC as the source. Make 'reverse recipes ' - reversing the source and destination tags. Then 'call ' that as a 'save recipe ' function.
Created Date: February 22,2012
Created by: jgargel
I am using the Recipe object to load recipes, but there is no similar object to save the tag values to existing recipes. I know i can use the Call Recipe object to do this, but that is less desirable. I have created graphical screens to change the recipe tag values and would like to save them to the current recipe without using the cumbersome Call Recipe object. Any way to do this? Can this be added as a feature request?