adccommunitymod (AutomationDirect) asked a question.

Reboot C-More

Created Date: December 29,2011

Created By: a agnone

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I think I read this issue several times now. I download an updated program to the C-More and it displays all my items on the main screen but will not respond to anything. I have to reboot the screen. I am downloading version 2.73 to see if that helps. I am running 2.72 on a 6 " c-more. After I download to the screen, I have to do a reboot from the software menu, then it works. This is the first time I had to do it repeatingly. I have had it happen in the past, but very random so I did not say anything. Now it is happening just about every time I download an updated program. All the items appear that I have on the main screen but all the items that display numbers are blank and none of the push buttons work. I do not get an error message at the top saying the plc is not communicating.


  • adccommunitymod (AutomationDirect)

    Created Date: January 03,2012

    Created by: HMI Eng

    Please provide the following information:

    1) Model of your C-more

    2) Are you using a CF in the CF1 slot?

    3) If the same project is downloaded to a different panel do you have the same issue?

    4) Does it happen with a different project in the same panel?

    You may need to contact Tech Support and provide your project for them to test.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: December 29,2011

    Created by: a agnone

    I think I read this issue several times now. I download an updated program to the C-More and it displays all my items on the main screen but will not respond to anything. I have to reboot the screen. I am downloading version 2.73 to see if that helps. I am running 2.72 on a 6 " c-more. After I download to the screen, I have to do a reboot from the software menu, then it works. This is the first time I had to do it repeatingly. I have had it happen in the past, but very random so I did not say anything. Now it is happening just about every time I download an updated program. All the items appear that I have on the main screen but all the items that display numbers are blank and none of the push buttons work. I do not get an error message at the top saying the plc is not communicating.

    Expand Post