adccommunitymod (AutomationDirect) asked a question.
Created Date: October 23,2011
Created By: a agnone
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I am using a 4 " micro. I set up the panel to plc to V2101. When I see the F-keys in the program, I get F1=1, F2=2 ' F3=4, F4=8, F5=10. V2101 is set to BCD in the tag database. So I went in and changed V2101 to Unassigned thinking i would see the key now at 1,2,4,8,16, but I do not. Key status is actually on V2102 for upper and V2103 for the lower keys. It seems changing V2100 to unassigned does not also change V2101 and V2102. V2101 and V2103 is automatically assigned. When doing the LED's, i set the V-memory to unassigned that way I get 1,2,4,8,16 etc. I was hoping I could do the same for key status.
Created Date: October 23,2011
Created by: a agnone
I am using a 4 " micro. I set up the panel to plc to V2101. When I see the F-keys in the program, I get F1=1, F2=2 ' F3=4, F4=8, F5=10. V2101 is set to BCD in the tag database. So I went in and changed V2101 to Unassigned thinking i would see the key now at 1,2,4,8,16, but I do not. Key status is actually on V2102 for upper and V2103 for the lower keys. It seems changing V2100 to unassigned does not also change V2101 and V2102. V2101 and V2103 is automatically assigned. When doing the LED's, i set the V-memory to unassigned that way I get 1,2,4,8,16 etc. I was hoping I could do the same for key status.