adccommunitymod (AutomationDirect) asked a question.

Cmore EA7-T8C (V2.71) PLC-499 Error code 0x0002

Created Date: September 07,2011

Created By: brianvanhouten

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I have the above cmore communicating with a P3-550 and have one screen with 18 numeric input objects. As soon the screen opens an error message reading "PLC-499: PAC - Error code 0x0002 return from plc " apears. The message goes away in a few seconds and never returns unless the screen is reopened. All entry objects were tagged using the plc export and the hmi import functions so i know all the tags are corrected and I also verified each object independently as far as functionality is concerned. When I go into the error log I see 15 of the 18 memory locations with a 4 byte error code. Any assistance on this would be very much appreciated.


  • adccommunitymod (AutomationDirect)

    Created Date: October 24,2011

    Created by: kvantal

    update fimware P3-550 to V.1.0.10.21

  • adccommunitymod (AutomationDirect)

    Created Date: January 12,2012

    Created by: automate-it

    Any suggestions when you 're running latest firmware and did a direct export from c-more and import to Productivity and still have the same problem? C-More v2.73

  • adccommunitymod (AutomationDirect)

    Created Date: January 12,2012

    Created by: kewakl

    see c-more help topic CM516.

    tag address problems

    I see this and :o assume that INSTANT that the tag is referenced, the HMI fails to recognize the tag/value in the pac

  • adccommunitymod (AutomationDirect)

    Created Date: September 07,2011

    Created by: brianvanhouten

    I have the above cmore communicating with a P3-550 and have one screen with 18 numeric input objects. As soon the screen opens an error message reading "PLC-499: PAC - Error code 0x0002 return from plc " apears. The message goes away in a few seconds and never returns unless the screen is reopened. All entry objects were tagged using the plc export and the hmi import functions so i know all the tags are corrected and I also verified each object independently as far as functionality is concerned. When I go into the error log I see 15 of the 18 memory locations with a 4 byte error code. Any assistance on this would be very much appreciated.

    Expand Post