adccommunitymod (AutomationDirect) asked a question.
Created Date: July 07,2011
Created By: wrumbaugh
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Have an application that I would like utilize the Click PLC (C0-01DR-D) real time clock and display date and time on the C-More Micro ( 3 IN, MICRO-GRAPHIC TCH PNL Part# EA1-S3ML). It does not appear that the C-More Micro has the built in option for Date and time like the C-More does. Either way would be acceptable. In either case besides displaying the real date and time I would also like to be able to turn on and off a piece of equipment, using the Click, at specific dates and times selectable by operator via input on C-more Micro. Is any of this possible with the CLICK and C-More Micro? Anyones help or recommendations is much appreciated. Thanks
Created Date: July 07,2011
Created by: bcarlton
Yes, there is enough information from the Real time clock so that the CMore Micro can display the relevant information and allow operators to enter the appropriate dates and times. it's all a matter of a lot of programming.
Dates and times are simply numbers. They can be read from the real time clock and compare to numbers entered by an operator. Depending on the compare you turn on or off outputs.
Do you need any specific help?
Created Date: July 07,2011
Created by: wrumbaugh
Have an application that I would like utilize the Click PLC (C0-01DR-D) real time clock and display date and time on the C-More Micro ( 3 IN, MICRO-GRAPHIC TCH PNL Part# EA1-S3ML). It does not appear that the C-More Micro has the built in option for Date and time like the C-More does. Either way would be acceptable. In either case besides displaying the real date and time I would also like to be able to turn on and off a piece of equipment, using the Click, at specific dates and times selectable by operator via input on C-more Micro.
Is any of this possible with the CLICK and C-More Micro?
Anyones help or recommendations is much appreciated.
Thanks