adccommunitymod (AutomationDirect) asked a question.
Created Date: December 16,2010
Created By: advctrl
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I have posted most of this before but hoping ..... 1) Make it so the Tag Name Database box can be re-sized. I would like it to be bigger so all the fields can be seen. 2) Once an editing box of any sort is re-sized, keep it that way so the next time it is opened it will come up the same. 3) Create a Arc tool 4) Allow Rounded Rectangles to be rotated. 5) Allow a group of objects to be rotated. 6) Create a multi-state color animation. ie - allow a rectangle to have say 20 colors, the color displayed will be determined by the value in a tag. 7) Object spacing tool. ie - If three or more objects are selected it will space them evenly between the outer most objects 8) Object centering tool. ie - If multiple objects are selected center them on a center point of all the objects selected. 9) Allow visibility to be added to a group of objects. 10) Allow Dynamic min / max values for numeric entry. ie - have the min / max point to tags in the plc 11) When an object is selected and zoom is clicked, zoom so the object is centered on the screen. 12) Add time stamp for when item alarmed and when it was cleared to alarm history screen. (info available when details pb is pressed) 13) Enable use of user defined keypad for passwords. 14) Allow user to create/customize the alarm history screen. 15) Allow all tag info to be edited.
Created Date: December 16,2010
Created by: advctrl
I have posted most of this before but hoping .....
1) Make it so the Tag Name Database box can be re-sized. I would like it to be bigger so all the fields can be seen.
2) Once an editing box of any sort is re-sized, keep it that way so the next time it is opened it will come up the same.
3) Create a Arc tool
4) Allow Rounded Rectangles to be rotated.
5) Allow a group of objects to be rotated.
6) Create a multi-state color animation. ie - allow a rectangle to have say 20 colors, the color displayed will be determined by the value in a tag.
7) Object spacing tool. ie - If three or more objects are selected it will space them evenly between the outer most objects
8) Object centering tool. ie - If multiple objects are selected center them on a center point of all the objects selected.
9) Allow visibility to be added to a group of objects.
10) Allow Dynamic min / max values for numeric entry. ie - have the min / max point to tags in the plc
11) When an object is selected and zoom is clicked, zoom so the object is centered on the screen.
12) Add time stamp for when item alarmed and when it was cleared to alarm history screen. (info available when details pb is pressed)
13) Enable use of user defined keypad for passwords.
14) Allow user to create/customize the alarm history screen.
15) Allow all tag info to be edited.