adccommunitymod (AutomationDirect) asked a question.

c-more bar graph- target line

Created Date: November 03,2010

Created By: sandhillcrane

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

waitng of the calendar year to change to buy a new c-more scrren and software, but does the c-more have a bar graph target line like the c-more micro? I need a target line that if it goes below it will signal. Any help or will I have to do this in two steps, overlaying the target? As always , thanks to yu guys who do this all time from those of us who dabble when the need hits.


  • adccommunitymod (AutomationDirect)

    Created Date: November 03,2010

    Created by: Bob S BN

    I had to open up a new micro project to see what you were talking about. :confused:

    I don't see a similar option in the regular c-more bar meter.:(

    Sorry,

  • adccommunitymod (AutomationDirect)

    Created Date: November 03,2010

    Created by: sandhillcrane

    waitng of the calendar year to change to buy a new c-more scrren and software, but does the c-more have a bar graph target line like the c-more micro? I need a target line that if it goes below it will signal. Any help or will I have to do this in two steps, overlaying the target? As always , thanks to yu guys who do this all time from those of us who dabble when the need hits.

    • rbenz (Customer)

      Started programming CM5 with version 9.02 and there's no target line option of the bar graph. What worse, is there's no way I can find to adjust the bar graph background, the graph having an section that's darken to ~7% when I simulate 100%

  • K Price (Customer)

    In the Bar/Circle Meter config box, scroll down to, and check, the Enable Alarm function. This allows you to set the alarm thresholds and the bar color to signal the alarm. You can use Static setpoints, or assign tags to the setpoints. (there are other display functions as well) Is this what you are looking for?