adccommunitymod (AutomationDirect) asked a question.

C-more and Web Server

Created Date: August 18,2010

Created By: mercedes98

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

The C-more touch panel has the ability to function as a Web Server. WHEN I LOG INTO THE PANEL (ea7-t8c) OVER THE WEB SERVER I DONT HAVE THE DEFAULT SCREEN. HOW DO I RESET WEB SITE TO "factory default " ?


  • adccommunitymod (AutomationDirect)

    Created Date: August 18,2010

    Created by: JoeW

    If I remember right, to change the Web Server screens you have to FTP into the panel and replace the index.html file. I don't think there is a way to reset only the web screens. IF you have another panel you could grab the index.html from it and put it in the panel in question. There may be an easier way I don't know of.

  • adccommunitymod (AutomationDirect)

    Created Date: August 18,2010

    Created by: Do-more PE

    Back up your project file from the panel if you haven't already done so.

    Press the upper left corner of the panel until it prompts for the system screen.

    Once in the system screen, select memory.

    Press "Reset To Factory Default. "

    Be aware that this will erase everything on the panel and restore it to factory condition. You will have to reload the project file as well as any custom HTML or other files that you may have previously loaded.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: August 18,2010

    Created by: mercedes98

    The C-more touch panel has the ability to function as a Web Server.

    WHEN I LOG INTO THE PANEL (ea7-t8c) OVER THE WEB SERVER I DONT HAVE THE DEFAULT SCREEN.

    HOW DO I RESET WEB SITE TO "factory default " ?