adccommunitymod (AutomationDirect) asked a question.

Adding ASCII text to Datalog

Created Date: June 21,2010

Created By: Jimbo

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I have a project that requires an alphanumeric serial number to be included in the data that is logged. The serial number is scanned from a barcode and placed into a ST register on an AB ML1100. I discovered today that the C-More won't allow ASCII to be datalogged. Are there any suggestions to how I could include the barcode? I would hate to abandon the C-More's datalogging capabilities to move the datalogging back to the limited space of the ML1100. Thanks, Jim


  • adccommunitymod (AutomationDirect)

    Created Date: June 22,2010

    Created by: Do-more PE

    If the serial number is actually numeric, you could move it to "N " registers and log it that way.

  • adccommunitymod (AutomationDirect)

    Created Date: June 23,2010

    Created by: Jimbo

    Response from Automation Direct Technical Support

    You can data log ASCII data by using a Lookup Text object and then embed a tag into the message that is tied to your ST register. You can then select this message to be data logged to the message database. This file will be a separate log file than the line trend graph.

  • adccommunitymod (AutomationDirect)

    Created Date: June 29,2010

    Created by: Hamilton Woods

    Adding ASCII text to Datalog

    Jimbo,

    The way I do this is through the alarm log. I add an alarm event that uses

    the same trigger as my data logging trigger (that logs the numeric data).

    One of the options for an Alarm event is to save the alarm file to USB. Since

    the alarm event is generated by the same trigger as the one that triggers

    logging the numeric data, the timestamp is essentially the same.

    I am logging approximately 60 fields, using 15 Line Trend Graph objects.

    After I ftp the results to a PC (I set up the C-More panel as an ftp server

    so that I can push recipes to it as well) I process the raw results files,

    including the alarm file and add a record for each trigger (in my case it is a

    test record). The ASCII fields all come from the alarm file.

    If you need more help, contact me.

    Hamilton Woods

    Accutrol, LLC

    HamiltonWoods@accutrol.com

    256-882-7433

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: June 21,2010

    Created by: Jimbo

    I have a project that requires an alphanumeric serial number to be included in the data that is logged. The serial number is scanned from a barcode and placed into a ST register on an AB ML1100.

    I discovered today that the C-More won't allow ASCII to be datalogged.

    Are there any suggestions to how I could include the barcode?

    I would hate to abandon the C-More's datalogging capabilities to move the datalogging back to the limited space of the ML1100.

    Thanks,

    Jim

    Expand Post