adccommunitymod (AutomationDirect) asked a question.
Created Date: June 09,2010
Created By: missouri100
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I just had a situation where I wanted the operators to read some text before pressing a particular button. I made a static text window and using the "advanced " option I made the text blink. It worked fine. The only problem was the response time for buttons already on the screen became very slow. The momentary buttons acted like toggle. When pressed, they stayed on. At first I reset them in my code. After I realized it might be the blinking text slowing it down and causing the momentary buttons to not work correctly, I turned off the blinking and everything went back to working fine. Has anyone else had this problem? If so, it makes blinking static text something that can't be used. thanks,
Created Date: June 12,2010
Created by: krak
I use the static text as an on screen alarm. I have not had this issue. Check that the setting on your buttons are in fact set to momentary. Otherwise I would assume that something else is causing a lag in the cmore. Which could either be the number of objects that need to be updated on the screen, or the communications cannot handle the traffic. If you are not already using Ethernet, try it and see if you get better results.
Created Date: June 15,2010
Created by: marksji
Also make sure you 're running the latest C-More programming software and the latest firmware in the panel. There was an issue years ago with what you 're describing, but its since been fixed.
Created Date: June 09,2010
Created by: missouri100
I just had a situation where I wanted the operators to read some text before pressing a particular button. I made a static text window and using the "advanced " option I made the text blink. It worked fine. The only problem was the response time for buttons already on the screen became very slow. The momentary buttons acted like toggle. When pressed, they stayed on. At first I reset them in my code. After I realized it might be the blinking text slowing it down and causing the momentary buttons to not work correctly, I turned off the blinking and everything went back to working fine.
Has anyone else had this problem? If so, it makes blinking static text something that can't be used.
thanks,