adccommunitymod (AutomationDirect) asked a question.
Lookout Direct ?
Created Date: April 15,2010
Created By: daakers
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I'm trying to get Direct Soft 5.3 to run from Lookout Direct Run menu. I'm using the same command line as the desktop icon but it does not load DS 5 in the applications of DSLaunch :confused: DSLaunch starts normal but without any of the apps. I go to the desktop icon and all loads correct. Here's the command line I'm using "C:\DirectSOFT5\Bin\DSLaunch.exe "
Created Date: April 15,2010
Created by: bcarlton
You'll also have to replicate the action of the 'start in ' parameter. Perhaps with a preliminary 'change directory '?
Created Date: April 15,2010
Created by: daakers
Thanks that done the trick :D
Created Date: April 15,2010
Created by: daakers
I'm trying to get Direct Soft 5.3 to run from Lookout Direct Run menu. I'm using the same command line as the desktop icon but it does not load DS 5 in the applications of DSLaunch :confused: DSLaunch starts normal but without any of the apps. I go to the desktop icon and all loads correct.
Here's the command line I'm using
"C:\DirectSOFT5\Bin\DSLaunch.exe "