adccommunitymod (AutomationDirect) asked a question.
Created Date: February 10,2010
Created By: duneman546
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I have several EZTouch programs on the old EZTouch panels. My customer bought some C-More panels because the EZTouch's are obsolete. I have purchased the C-More panels and I need to convert the EZTouch programs to C-More, however the EZTouch software I used to create the programs was version 2.2. C-More does not seem to want to "play ball " with any version under 3.1. Is there any way to convert them over? Can I get an updated version of EZTouch and upgrade the programs to 3.1 first, then convert? Please help, I don't want to have to start from scratch. Thanks.
Created Date: February 10,2010
Created by: Rich19551
Call these people and see if they can help.
http://flash.ezautomation.net/
Created Date: February 12,2010
Created by: HMI Eng
I recommend you call tech support. They maybe able to help. Do you have the 2.2 EZTouch software where you can read the projects from the panels?
Created Date: February 10,2010
Created by: duneman546
I have several EZTouch programs on the old EZTouch panels. My customer bought some C-More panels because the EZTouch's are obsolete. I have purchased the C-More panels and I need to convert the EZTouch programs to C-More, however the EZTouch software I used to create the programs was version 2.2. C-More does not seem to want to "play ball " with any version under 3.1.
Is there any way to convert them over? Can I get an updated version of EZTouch and upgrade the programs to 3.1 first, then convert?
Please help, I don't want to have to start from scratch.
Thanks.