adccommunitymod (AutomationDirect) asked a question.

Max C-More's

Created Date: June 22,2009

Created By: daakers

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

How many C-More panels can you connect to a PLC without problems. I 've been able to do 3 in the past without any issues. We now have a project that will require 6 C-More's to 1 PLC over ethernet connection. What issues if any will I run into? Thanks ahead for any help :)


  • adccommunitymod (AutomationDirect)

    Created Date: June 22,2009

    Created by: Do-more PE

    It all depends on how much data you are putting through the connection. 6 could be ok, but then it also depends on how many registers you will be requesting that are not contiguous.

    There isn't a hard and fast rule for the number of connections you can have because of all of the variables.

    If you are doing any communications out of the Ethernet port(s) on the PLC(s) to devices other than Cmore than that will make a difference as well. So will how busy the network is. There are just too many variables to say, "X is the number that you can connect. "

    All of that being said, we have tested more than 6 connections with no issues but we can't guarantee that will be the case for you.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: June 23,2009

    Created by: daakers

    Thanks

    It all depends on how much data you are putting through the connection. 6 could be ok, but then it also depends on how many registers you will be requesting that are not contiguous.

    There isn't a hard and fast rule for the number of connections you can have because of all of the variables.

    If you are doing any communications out of the Ethernet port(s) on the PLC(s) to devices other than Cmore than that will make a difference as well. So will how busy the network is. There are just too many variables to say, "X is the number that you can connect. "

    All of that being said, we have tested more than 6 connections with no issues but we can't guarantee that will be the case for you.

    Thanks for the fast reply. I think we'll be good then. Only about 50 or so tags per C-More and maybe a couple product counts for each.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: June 22,2009

    Created by: daakers

    How many C-More panels can you connect to a PLC without problems. I 've been able to do 3 in the past without any issues. We now have a project that will require 6 C-More's to 1 PLC over ethernet connection.

    What issues if any will I run into?

    Thanks ahead for any help :)