adccommunitymod (AutomationDirect) asked a question.

Using the C-More Micro-Graphic Bezel

Created Date: May 25,2009

Created By: rlcrewse

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I'm using a 20-Key Bezel with a C-more 3 " Micro-Graphic Display. (EA1-S3ML-N & EA-MG-BZ2). I'm using a Numeric Entry object to allow me to change the preset for a timer. The Data Entry Tag refers to V1300 as its data point and F1 as the initiator of the Function key assignment. I 've setup the timer in a DL06 PLC using V1300 as the preset. When I connect the PLC and display the Data Entry object reads the timer preset OK. I can change the preset while online with DirectSoft 5 and watch it change on the display so the comms setup is OK. I can select F1 on the display and the object goes to its data entry mode. However, none of the keys on the 20-Key Bezel has any affect on the display or memory location! I noticed in the C-More Micro software (Ver 2.20.0.0) that you can enable/disable sending the current key status of the bezel. Is this necessary for the keypad to function? If so, are there examples of how to write a keypad routine in RLL in the PLC to make this keypad work. Any help/guidance will be greatly appreciated, Thanks


  • adccommunitymod (AutomationDirect)

    Created Date: May 25,2009

    Created by: rlcrewse

    Problem Found!

    It turns out that I was being too delicate in mounting the C-More Micro-Graphic display into the bezel. I was afraid of over-tightening the mounts and breaking the plastic case. I removed all but about a 1/32 " of a gap between the two bodies and every thing started to work fine.

    I have only one minor design complaint about the keyboard function and Data Entry. When an object is selected I should be able to key in the new data and hit enter for the change to take affect. But it appears that you have to hit "CLR " to clear out the setting before you can make a change. Its a small thing but its an extra step that the production operators will have to be made aware of.

    Other than that this seems like a nice little HMI for simple applications. The ability to change or flash the different backlighting colors is great for getting an operator's focus of attention.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: May 26,2009

    Created by: HMI Eng

    I have only one minor design complaint about the keyboard function and Data Entry. When an object is selected I should be able to key in the new data and hit enter for the change to take affect. But it appears that you have to hit "CLR " to clear out the setting before you can make a change. Its a small thing but its an extra step that the production operators will have to be made aware of.

    Check the next release. It is being added as a selection in the panel manager to clear or not clear. Keep an eye on the website and make sure you have signed up for update notification.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: May 25,2009

    Created by: rlcrewse

    I'm using a 20-Key Bezel with a C-more 3 " Micro-Graphic Display. (EA1-S3ML-N & EA-MG-BZ2). I'm using a Numeric Entry object to allow me to change the preset for a timer. The Data Entry Tag refers to V1300 as its data point and F1 as the initiator of the Function key assignment. I 've setup the timer in a DL06 PLC using V1300 as the preset. When I connect the PLC and display the Data Entry object reads the timer preset OK. I can change the preset while online with DirectSoft 5 and watch it change on the display so the comms setup is OK. I can select F1 on the display and the object goes to its data entry mode. However, none of the keys on the 20-Key Bezel has any affect on the display or memory location! I noticed in the C-More Micro software (Ver 2.20.0.0) that you can enable/disable sending the current key status of the bezel. Is this necessary for the keypad to function? If so, are there examples of how to write a keypad routine in RLL in the PLC to make this keypad work.

    Any help/guidance will be greatly appreciated,

    Thanks

    Expand Post