adccommunitymod (AutomationDirect) asked a question.

Multiple alarms using c-more micro

Created Date: December 18,2008

Created By: Paddington

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Hi I´m programing a ventilation system that will be operated using a c-more micro panel and I´m wondering if I the Micro has anything like the alarm log in the c-more program. I´m using the method described in the webinar on the alarm function, where I load the alarm number into v3000 and use a look up text box to display the alarm in the alarm control setup. I´d rather not have to create a ladder queue to store unacknowledged alarms until the first alarm is cleared. Any bright ideas? Thx Doddi


  • adccommunitymod (AutomationDirect)

    Created Date: December 18,2008

    Created by: OpZed

    C-micro has no clock for logging, it will only display active alarms.

  • adccommunitymod (AutomationDirect)

    Created Date: December 18,2008

    Created by: Paddington

    Hi

    I´m programing a ventilation system that will be operated using a c-more micro panel and I´m wondering if I the Micro has anything like the alarm log in the c-more program.

    I´m using the method described in the webinar on the alarm function, where I load the alarm number into v3000 and use a look up text box to display the alarm in the alarm control setup.

    I´d rather not have to create a ladder queue to store unacknowledged alarms until the first alarm is cleared.

    Any bright ideas?

    Thx

    Doddi

    Expand Post