adccommunitymod (AutomationDirect) asked a question.

CMORE Micro recipe function

Created Date: October 24,2008

Created By: Tubecut

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Is there a method to have the PLC generate a recipe action. It seems that there must be a recipe button to cause the function to activate. I have six lookup text to display when navigating to a screen and I would like the text to be on the screen when navigating there. I also don't think I want to use a function key but if that is the way..... Is there a better way to accomplish this with out having the PLC control the look up text to display the six different look up the text box and the associated tags which display additional numeric data. These are six different look up text displays. Thanks in advance.


  • adccommunitymod (AutomationDirect)

    Created Date: October 24,2008

    Created by: Tubecut

    Is there a method to have the PLC generate a recipe action. It seems that there must be a recipe button to cause the function to activate.

    I have six lookup text to display when navigating to a screen and I would like the text to be on the screen when navigating there. I also don't think I want to use a function key but if that is the way.....

    Is there a better way to accomplish this with out having the PLC control the look up text to display the six different look up the text box and the associated tags which display additional numeric data. These are six different look up text displays.

    Thanks in advance.

    Expand Post