adccommunitymod (AutomationDirect) asked a question.

C-More USB Driver Problem

Created Date: June 23,2008

Created By: pharrison

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I'm having an issue getting the C-More USB Driver to install on my XP SP2 machine. I tried it on another machine and it worked fine. I contacted tech support, and I was told to re-install windows. I have multiple USB devices on this PC that work fine, and as recently as yesterday I have successfully installed other USB Drivers for other devices without a problem. I 've tried uninstalling/reinstalling multiple times; all while making sure the unit is unplugged during the install process. Ultimately I end up with the 'Cannot Install this Hardware ' message. Under device manager, the device 'EA7 Operator Interface ' is marked with an exclamation point. Has anyone out there had this problem? Any ideas? Thanks for your help!


  • adccommunitymod (AutomationDirect)

    Created Date: June 24,2008

    Created by: automate-it

    I know it sounds simple, but have you tried using a different USB port? I have some devices that won't work on my front USB ports, but work fine on the back.

  • adccommunitymod (AutomationDirect)

    Created Date: June 24,2008

    Created by: pharrison

    So far I 've tried 2 ports in the front, and 2 ports in the back. No luck.

    Thanks for the suggestion!

  • adccommunitymod (AutomationDirect)

    Created Date: June 24,2008

    Created by: allukes

    The problem that I have run into is that other programs are reserving the COM ports on startup. You said that you had many other USB devices. Perhaps they are blocking the installation software from using a port. I can't remember what the port range is on the USB adapter driver. Some are limited to the first 8.

  • adccommunitymod (AutomationDirect)

    Created Date: June 25,2008

    Created by: pharrison

    I was finally able to get it to work. I upgraded from v2.0 to v2.1. I uninstalled the device in device manager, and plugged the unit back in to reinstall it. It still did not install, so I manually pointed it to the driver file, and it installed fine.

    Oddly enough, I did this same thing multiple times in v2.0 without any success.

    allukes, I did uninstall some of my USB devices. It still didn't work in v2.0, but maybe it contributed to my success in v2.1? Thanks for the helpful suggestions.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: July 02,2008

    Created by: HMI Eng

    There was an issue with versions previous to version 2.1 . As you found out it is fixed in 2.1.

  • adccommunitymod (AutomationDirect)

    Created Date: June 23,2008

    Created by: pharrison

    I'm having an issue getting the C-More USB Driver to install on my XP SP2 machine. I tried it on another machine and it worked fine. I contacted tech support, and I was told to re-install windows. I have multiple USB devices on this PC that work fine, and as recently as yesterday I have successfully installed other USB Drivers for other devices without a problem. I 've tried uninstalling/reinstalling multiple times; all while making sure the unit is unplugged during the install process. Ultimately I end up with the 'Cannot Install this Hardware ' message. Under device manager, the device 'EA7 Operator Interface ' is marked with an exclamation point.

    Has anyone out there had this problem? Any ideas? Thanks for your help!

    Expand Post