adccommunitymod (AutomationDirect) asked a question.
Created Date: May 28,2008
Created By: wernerk
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I have a project that will involve monitor the water level in three tanks and I need to be able to change the set point values for a HI level alarm, Low level Alarm, Pump Call setpoint, and Pump Stop setpoint. The OP-413 Setpoint Display panel works great when I am only dealing with one site, but I need to control 3 sites. The OP-1312 would have worked, but it lacks one more setpoint control per site. Is there a better panel to use for this function, would the C-More line fit the bill. I am using a DL06 PLC as the Master PLC and control in this system.
Created Date: May 28,2008
Created by: KPrice
wernerk, yes, the C-more is definitely the way to go. It is so much easier and much more powerful than the OP panels. You can have a lot of setpoints and have a lot of fun along the way.
Created Date: May 28,2008
Created by: 72hdflh
Originally posted by KPrice:
wernerk, yes, the C-more is definitely the way to go. It is so much easier and much more powerful than the OP panels. You can have a lot of setpoints and have a lot of fun along the way.
I agree!
Created Date: May 28,2008
Created by: wernerk
I have a project that will involve monitor the water level in three tanks and I need to be able to change the set point values for a HI level alarm, Low level Alarm, Pump Call setpoint, and Pump Stop setpoint. The OP-413 Setpoint Display panel works great when I am only dealing with one site, but I need to control 3 sites. The OP-1312 would have worked, but it lacks one more setpoint control per site. Is there a better panel to use for this function, would the C-More line fit the bill. I am using a DL06 PLC as the Master PLC and control in this system.