adccommunitymod (AutomationDirect) asked a question.
Created Date: August 15,2007
Created By: a agnone
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I have not dug into it yet, but I would like to know if the panel can tell when it has completed playing an audio file? If the panel is playing, "warning, temperature is too high " and another event triggers another audio message, will the C-more wait until it finishes the first one or will it cut it off and play the next one? Would be nice to have a bit from the panel saying it has finished the audio file, and use that bit to trigger the next. I am now just setting up a C-More with audio messages, not finished yet.
Created Date: August 15,2007
Created by: a agnone
I have not dug into it yet, but I would like to know if the panel can tell when it has completed playing an audio file? If the panel is playing, "warning, temperature is too high " and another event triggers another audio message, will the C-more wait until it finishes the first one or will it cut it off and play the next one? Would be nice to have a bit from the panel saying it has finished the audio file, and use that bit to trigger the next. I am now just setting up a C-More with audio messages, not finished yet.