adccommunitymod (AutomationDirect) asked a question.

C-more micro blank screen

Created Date: June 13,2007

Created By: a agnone

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I had a machine powered up and plugged the micro into the 2nd port. Using a DL240 with DirectNet at the fasted baud for that CPU. The micro lit up but nothing displayed. I unplugged it and plugged it back into port 2 and it worked. This has happened couple times at various times. Is it okay to plug the micro into a powered up CPU? Do I need to power down the machine before plugging in the micro to the port?


  • adccommunitymod (AutomationDirect)

    Created Date: June 16,2007

    Created by: Kristjan H

    You don't need to power down the machine before plugging in the micro.

    The OP displays have had similar issues and I don't know the reason for it. Are you using a homemade cable? You know the cable shouldn't be more than 10 feet on serial RS-232.

    Why can't I find any information in the manual about baud rate for the C-More Micro? What is the baud rate? Are you sure the Micro and PLC port communication settings are the same?

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: June 22,2007

    Created by: a agnone

    The micro and the plc are 1 foot away. It hasn't done it lately. It only happened when the machine was powered up, I unplugged the micro to change the program, then plugged it back in back into the plc port, the screen stayed blank (green light, no words). I unplugged the micro then plugged it back into the plc and it came up okay. It did it on that machine and another.

  • adccommunitymod (AutomationDirect)

    Created Date: June 13,2007

    Created by: a agnone

    I had a machine powered up and plugged the micro into the 2nd port. Using a DL240 with DirectNet at the fasted baud for that CPU. The micro lit up but nothing displayed. I unplugged it and plugged it back into port 2 and it worked. This has happened couple times at various times. Is it okay to plug the micro into a powered up CPU? Do I need to power down the machine before plugging in the micro to the port?

    Expand Post