adccommunitymod (AutomationDirect) asked a question.

text not coming through to HMI

Created Date: June 11,2007

Created By: nuf

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I am new to using Automation Direct. I am sure I 've overlooked something simple, but I am using a VPRINT box on a DL06 to write System Errors to V-mem. I am then putting the V-mem location on the LCD at the panel. So far works fine. The problem is when I try to also put the Error into a Dynamic Text box on the C-more. I get a little square character instead of the text. Only a problem for the HMI, LCD reads fine. I can use the DataView tool in DS5 to write text to the memory location and everything works fine, the message is displayed on LCD and HMI. Is there a trick to using VPRINT, or is there another way to do this that would be better.


  • adccommunitymod (AutomationDirect)

    Created Date: June 11,2007

    Created by: nuf

    I am new to using Automation Direct.

    I am sure I 've overlooked something simple, but I am using a VPRINT box on a DL06 to write System Errors to V-mem. I am then putting the V-mem location on the LCD at the panel. So far works fine. The problem is when I try to also put the Error into a Dynamic Text box on the C-more. I get a little square character instead of the text. Only a problem for the HMI, LCD reads fine.

    I can use the DataView tool in DS5 to write text to the memory location and everything works fine, the message is displayed on LCD and HMI.

    Is there a trick to using VPRINT, or is there another way to do this that would be better.

    Expand Post