adccommunitymod (AutomationDirect) asked a question.
Created Date: June 07,2007
Created By: mytekcontrols
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I am previewing the C-more micro touch panel programming application software (Version 1.12.7.15a). While creating a couple screens, I encountered the following error when I was trying to save the file: Error GUI-177: Device Limit Exceeded. Device cannot be added to project. Max limit is 1 for device. This seemed to occur just after I had placed a "RUN " and "STOP " button object, and then tried to save the project (previous saves had been done without incident). So I deleted these 2 objects from the screen and also from the database, and once again tried to save the project. Same error message came up. The interesting thing is that the file is being saved, and when later opened, the updates will appear. However each time the file is re-opened, I also get the same error message. This also occurs when trying to simulate the project, although it doesn't seem to interfere with the simulation working. I am truly puzzled as to what to do, or what I may have done to cause this.
Created Date: June 08,2007
Created by: Tech Guy
Please call Technical Support at 1(800)633-0405 or (770)844-4200.
Created Date: June 08,2007
Created by: mytekcontrols
"Please call Technical Support "
Thanks, but I think I could have figured that out myself.
I really think it would be far more useful to myself, and others, if we covered the topic here online. After all isn't that the purpose of this forum?
Created Date: June 10,2007
Created by: franji1
Actually, the purpose is to solve problems. Another critical purpose is to help educate the masses, but it does not trump the main purpose (unless this was an academic exercise).
I recommend you call Technical Support - there are more/better ways to solve issues than posted text on a web page. Forums are excellent for very asynchronous problem solving of many problems, but not ALL problems.
If you get your problem solved, then it would be GREAT if you posted the solution back here, along with any caveats, gotchas, how you got to the solution, etc. (You'd be suprised how many people do NOT do this, so your goal is admirable!)
Trust me, if someone named "Tech Guy " recommends you call tech support, it's probably a really good idea. http://forum1.automationdirect.com/board/biggrin.gif
Created Date: June 10,2007
Created by: mytekcontrols
Yes I will call Tech Support, and yes I will gladly share what I find out about the problem.
I take it that Tech Guy must know his stuff, by what you implied with your final comment. So I must have hit upon an unusual problem. This can be both good and bad. Good that I am one of the few, and bad because it picked me to reveal itself.
Created Date: June 11,2007
Created by: franji1
Originally posted by mytekcontrols:
I take it that Tech Guy must know his stuff, by what you implied with your final comment.
Yes, it's one of the ADC tech guys who constantly monitor the forum.
So I must have hit upon an unusual problem. This can be both good and bad. Good that I am one of the few, and bad because it picked me to reveal itself.
That's exactly what I was thinking!
We at Host Engineering (developers of DirectSOFT) can solve a lot of problems using the Forum, but sometimes it's a strange enough problem where a phone call or possibly an email (to send files back and forth) is the only way we 're gonna figure out the problem.
Created Date: June 27,2007
Created by: mytekcontrols
It's been a while, so I thought I'd update everyone on this issue.
I have been rather busy lately and wasn't able to contact tech support until today (besides I hate waiting while on hold, and had to clear aside some time to do so).
The support tech I talked with was Victor, and he was unable to find a reference to such an error ever occurring before. I was asked to email the file to the programming section at Automation Direct, in order for them to get a better handle on what is going wrong (I sent the file today).
When I get a response I'll post it here (might be a new version of software coming).
Created Date: June 27,2007
Created by: mytekcontrols
Fast Response!!!!
Victor just called me back from Tech Support, and said he had found the problem. Apparently I had too many protocols set-up under the Com Port selection.
To check and fix this problem, I went to "Setup - Panel Manager " from the C-more applications menu bar.
Here's what came up:
Panel (EA1-S3ML)
Com Port1
DEV001 (highlighted green)
DEV001(1)
DEV001(2)
The first DEDV001 that was highlighted in green was set to Modbus RTU, which is the communications mode that I had originally setup for the C-more Micro Panel. The other two were set as DirectLogic K-Sequence. Now unless I am mistaken, I don't recall doing anything that should have created these other two entities. The good news is that by simply selecting DEV001(1) and DEV001(2), deleting , and then choosing "Save " when closing the Panel Manager, all is well.
Victor says they'll be looking into the slight possibility that something attributed to the use of the STOP and RUN button objects might have inadvertently caused additional Com Port DEV's to occur.
Of course there is always the possibility that being new to using the software, I goofed somewhere, and I am the actual cause of the problem.
Created Date: November 03,2010
Created by: redbinary
still an issue
I know this thread started 3 years ago but I had the same issue with a project for an EA1-T6CL after just looking through the library objects just to see what they were. I added 3 or 4 then immediately deleted them. Thanks to this thread I knew to look in the set-up menu. Sure enough there was a superfluous "device " for each library object I had added.
:Patrick
Created Date: November 04,2010
Created by: a agnone
How funny an old post can be so helpful. I just got a GUI error and just ignore it. hahaha I will have to do the same check. I will have to get the number of the GUI error. I'll come back and post it.
Created Date: June 09,2013
Created by: iadapt
It Worked For Me!
Thanks this forum post helped me quickly within just 1 minute I solved my problem. Not the usual experience with computer issues. Thanks guys.