adccommunitymod (AutomationDirect) asked a question.

Wireless ethernet interface

Created Date: January 17,2007

Created By: 2004sk4

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Is there a way or product that i can use to wirelessly connect to a freestanding c-more touch screen. The plant I work at has wired and wireless network. The idea that has been kicked around is. Hook a 8 " touchscreen to the serial port of the plc to control the machine while using the panel pass through function to communicate to a remote wireless 6 " hmi located and powered on the maint. cart. The data captured would allow us to know immediately when a machine goes down and possibly what caused it depending on the plc program.


  • adccommunitymod (AutomationDirect)

    Created Date: January 17,2007

    Created by: 2004sk4

    Is there a way or product that i can use to wirelessly connect to a freestanding c-more touch screen. The plant I work at has wired and wireless network.

    The idea that has been kicked around is.

    Hook a 8 " touchscreen to the serial port of the plc to control the machine while using the panel pass through function to communicate to a remote wireless 6 " hmi located and powered on the maint. cart.

    The data captured would allow us to know immediately when a machine goes down and possibly what caused it depending on the plc program.

    Expand Post