adccommunitymod (AutomationDirect) asked a question.
Created Date: December 19,2006
Created By: sgsims
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
If I setup a selector switch on a C-More Panel with a tag to say C20 bit what happens upon return from a power cycle? For example: If I use the touch screen to turn the selector switch ON thus making the C0 bit go to 1 if I cycle the power will the C-More screen still show that selector switch in the ON position? If that is not the case if I make the C20 a retentive bit will the C20 being a 1 upon start-up cause the selector switch on the C-more panle to be in the ON position?
Created Date: January 26,2007
Created by: ICS
Non-retentive values will revert to zero following a power cycle. Retentive values will retain their value and correctly propogate them to the display.
Created Date: December 19,2006
Created by: sgsims
If I setup a selector switch on a C-More Panel with a tag to say C20 bit what happens upon return from a power cycle?
For example: If I use the touch screen to turn the selector switch ON thus making the C0 bit go to 1 if I cycle the power will the C-More screen still show that selector switch in the ON position? If that is not the case if I make the C20 a retentive bit will the C20 being a 1 upon start-up cause the selector switch on the C-more panle to be in the ON position?