adccommunitymod (AutomationDirect) asked a question.

Downloading new program to C-More Micro

Created Date: October 04,2006

Created By: sdsmith

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I haven't acquired a unit yet, but was wondering if a new program can be installed similiar to the way you can email a program to a customer using DNLoader for AD-PLCs (ie a DNLoader program for the C-More Micro)? This would be useful whenever a customer asked for a change in the panel. Thanks Sean


  • adccommunitymod (AutomationDirect)

    Created Date: October 04,2006

    Created by: Steven

    I don't think there is a standalone program like DNLoader for loading binaries to the panel, but there's an alternative.

    Since the CMore Micro programming IDE is free and easy to download, you could have the end user install it and use it to update their panels. You can use the option Save Project As Protected to prevent them from editing the project; it should only allow them to send it to the panel without opening it for editing, if I understand it correctly.

    Of course, the user would have to have access to the panel, and a CMore Micro programming cable for this to work.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: October 05,2006

    Created by: sdsmith

    Thanks Steven

  • adccommunitymod (AutomationDirect)

    Created Date: October 04,2006

    Created by: sdsmith

    I haven't acquired a unit yet, but was wondering if a new program can be installed similiar to the way you can email a program to a customer using DNLoader for AD-PLCs (ie a DNLoader program for the C-More Micro)? This would be useful whenever a customer asked for a change in the panel.

    Thanks

    Sean

    Expand Post