adccommunitymod (AutomationDirect) asked a question.
Created Date: February 06,2006
Created By: JavierSosa
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I 've had trouble with C-more corrupting the project I'm working on. The first 2 times it happened I got the error message ????? 'BORLNDMM.DLL '????? 011943BB ????? 0C186C5C ?????????????????. Then I closed c-more and when I tried to reopen the project is said that an error had occured and c-more would have to be restarted. The other 5 or so times it happened it was without warning. I would try to open a project that I thought was complete, then the error would pop up, causing me to lose hours or work each time. The only thing I can do now, is save the project, close the program, try to open the project, if successful, copy the program to a different folder, and use that as a back up. As you can imagine this is pretty tedious. If you can give any insight as to why this is happening, that would be great. Also, I 've tried to recreate the error on purpose, and I cannot find any series of actions that cause it to happed. There was one time, after the project was corrupted, I kept on trying to open it, then I tried to import screens from the project into a new project, some screens would transfer just fine, but others screens would cause the program to crash as usual. But, randomly it started working again, but all the font styles and sizes were different from what I initially set them as. Thanks Javier
Created Date: February 07,2006
Created by: clasentech
I know this really doesn't help but see the first and last comment in this link.
http://forum1.automationdirect.com/board/Forum8/HTML/000092.html
Created Date: February 07,2006
Created by: clasentech
The only thing tech support did for me on the phone was suggest I upgrade to service pack 2 for XP. I did that, but because of all the various lost time I'm still affraid to use C-More on that laptop. I had C-more uninstalled, re-installed, several times. Sometimes it would work, usually it didn't.
Created Date: March 23,2006
Created by: Tech Guy
This is possibly a bug we have found. The project file is corrupted if you press "Send " right after saving the file the file has not completed saving before it sends it to the panel, therefore it gets corrupted.
Created Date: February 06,2006
Created by: JavierSosa
I 've had trouble with C-more corrupting the project I'm working on.
The first 2 times it happened I got the error message
????? 'BORLNDMM.DLL '????? 011943BB ????? 0C186C5C ?????????????????.
Then I closed c-more and when I tried to reopen the project is said that an error had occured and c-more would have to be restarted.
The other 5 or so times it happened it was without warning. I would try to open a project that I thought was complete, then the error would pop up, causing me to lose hours or work each time.
The only thing I can do now, is save the project, close the program, try to open the project, if successful, copy the program to a different folder, and use that as a back up. As you can imagine this is pretty tedious.
If you can give any insight as to why this is happening, that would be great.
Also, I 've tried to recreate the error on purpose, and I cannot find any series of actions that cause it to happed.
There was one time, after the project was corrupted, I kept on trying to open it, then I tried to import screens from the project into a new project, some screens would transfer just fine, but others screens would cause the program to crash as usual.
But, randomly it started working again, but all the font styles and sizes were different from what I initially set them as.
Thanks
Javier