adccommunitymod (AutomationDirect) asked a question.
Touch screen simulator
Created Date: January 27,2006
Created By: todd1313
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I was just wondering if it is possible to set-up my PC as a "touch screen " in place of the real Ez-touch screen? My boss and I are trying to work on the same project but he has the actual screen. I have the EZ-touch program but was wondering if I could use my mouse and my monitor as the 'touch. ' thanks, Todd
Created Date: January 27,2006
Created by: marksji
Unfortunetly, no.
Created Date: January 27,2006
Created by: todd1313
OK, Thanks
Created Date: January 27,2006
Created by: jackson
You can simulate the project by selecting the Simulate option above the pallette.
It will not actually write to the PLC, but it does come up with a tag database simulator to show the values of the tags.
Created Date: January 27,2006
Created by: marksji
The EZ-Touch doesn't have that button; only the C-More.
Created Date: January 28,2006
Created by: jackson
Oops...sorry about that. I got my topics mixed up I guess.
Created Date: January 27,2006
Created by: todd1313
I was just wondering if it is possible to set-up my PC as a "touch screen " in place of the real Ez-touch screen? My boss and I are trying to work on the same project but he has the actual screen. I have the EZ-touch program but was wondering if I could use my mouse and my monitor as the 'touch. '
thanks,
Todd