adccommunitymod (AutomationDirect) asked a question.

EZtouch Recipe

Created Date: September 06,2005

Created By: rrdoyle

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Is there a way to save input data from one screen to different Recipe Buttons? Lets say I have a Main Screen with several user input parameters and want to save these to a Recipe Button 1 to be recalled later. I believe that I can do this with Source from Another Tag in the Recipe Button setup. Can I input new data in the Main Screen and direct it to Recipe Button 2? If this is possible, how is it done?


  • adccommunitymod (AutomationDirect)

    Created Date: September 06,2005

    Created by: bcarlton

    The standard view of a recipe button is to store a set of preset numbers into PLC register locations. The EZTouch allows the source to be another register location. So think of this button as a general register transfer function. If you have a set of recipe buttons with their sources and destinations set up then do another screen with the same recipe buttons but with the source and destination swapped. These will be 'save recipe ' buttons. I even used recipe buttons when I needed to zero out a group of locations at a button push. I just loaded a constant 0 into the registers. Don't let the name 'recipe ' blind you to what the button can actually do.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: September 06,2005

    Created by: rrdoyle

    Is there a way to save input data from one screen to different Recipe Buttons?

    Lets say I have a Main Screen with several user input parameters and want to save these to a Recipe Button 1 to be recalled later. I believe that I can do this with Source from Another Tag in the Recipe Button setup. Can I input new data in the Main Screen and direct it to Recipe Button 2? If this is possible, how is it done?

    Expand Post