adccommunitymod (AutomationDirect) asked a question.

10" EZ-Touch Pedestal

Created Date: February 03,2005

Created By: marksji

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

We 're thinking of making up some pedestals to fit the 10 " EZ-Touch screens and I'm curious if anyone would be interested in buying a few. We 're trying to get the quantities up enough to get the manufacturing costs down to a reasonable level. Also does anyone have suggestions for what they 've used in the past? Below is a description of what the pedestals we 're working on will look like (pulled from an email). I'll post a pic as soon as the prototype is finished. >This would be a box for the touch screen >that pivots at 3 different angles. >Connection plugs (Ethernet & 120VAC, 24V >power supply included in the pedestal) will >be mounted on the box, eliminating the need >for conduit. A 3 x 3 tube provides >vertical support. It is bolted (not >welded, for easier shipping) to a 20 x 20 >base plate with leveling feet. The tube >will also serve as the conduit for Ethernet >cable and 120 VAC plug. The assembly will >be powder-coated a textured black...it >looks pretty high-tech. I think it will >make a nice pedestal, particularly for >secondary screens in offices, but also for >overcrowded consoles.


  • adccommunitymod (AutomationDirect)

    Created Date: February 03,2005

    Created by: marksji

    We 're thinking of making up some pedestals to fit the 10 " EZ-Touch screens and I'm curious if anyone would be interested in buying a few. We 're trying to get the quantities up enough to get the manufacturing costs down to a reasonable level. Also does anyone have suggestions for what they 've used in the past? Below is a description of what the pedestals we 're working on will look like (pulled from an email). I'll post a pic as soon as the prototype is finished.

    >This would be a box for the touch screen

    >that pivots at 3 different angles.

    >Connection plugs (Ethernet & 120VAC, 24V

    >power supply included in the pedestal) will

    >be mounted on the box, eliminating the need

    >for conduit. A 3 x 3 tube provides

    >vertical support. It is bolted (not

    >welded, for easier shipping) to a 20 x 20

    >base plate with leveling feet. The tube

    >will also serve as the conduit for Ethernet

    >cable and 120 VAC plug. The assembly will

    >be powder-coated a textured black...it

    >looks pretty high-tech. I think it will

    >make a nice pedestal, particularly for

    >secondary screens in offices, but also for

    >overcrowded consoles.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: February 11,2005

    Created by: a agnone

    Interesting, we made our own by simpling using a Rittal cabinet that fits the display. Then cut a stainless steel pipe about 2 " diameter, then making a angle piece to fit the tube to the cabinet. The base is made out of aluminum and swivels 160. The wires pass through the tube to the machine.