adccommunitymod (AutomationDirect) asked a question.
Created Date: May 14,2004
Created By: twbrock
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
On an existing system, not mine, there is the following: D4-440 on an 8-slot base 6 D4-16TR in slots 0-5 2 D4-DCM in slots 6 & 7 D4-EX on 8-slot base 3 D4-16TR in slots 0-2 3 TCP Quick Panel Jr. One of the Quick Panels has gone out completely and is now not working. What I want to do is replace the 3 QPJ with EZ-Touch Panels. I know I have to remake the cables. The problem is with the DCM’s the manual says that ‘each station must have a unique address’ but the existing system has both set on 01 HEX and it works now?????? Any ideas! Thanks Tommy
Created Date: May 14,2004
Created by: franji1
I'm pretty sure that if each DCM is on its own separate network (it's own wire), they can have the same "address ".
Created Date: May 14,2004
Created by: twbrock
On an existing system, not mine, there is the following:
D4-440 on an 8-slot base
6 D4-16TR in slots 0-5
2 D4-DCM in slots 6 & 7
D4-EX on 8-slot base
3 D4-16TR in slots 0-2
3 TCP Quick Panel Jr.
One of the Quick Panels has gone out completely and is now not working. What I want to do is replace the 3 QPJ with EZ-Touch Panels. I know I have to remake the cables. The problem is with the DCM's the manual says that "each station must have a unique address' but the existing system has both set on 01 HEX and it works now?????? Any ideas!
Thanks
Tommy