adccommunitymod (AutomationDirect) asked a question.

EZTouch 2.0 Error Message

Created Date: April 16,2002

Created By: khfok

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Recently I upgraded my EZtouch editor software to 2.0. After I used it to create an application, next time when I try to reopen it, the program showed an error mesage saying that "Error S01_2: EZTouch editor detected that one or more objects ... outside the 320x240 resolution, ... " But my screen and all objects are fine and within the 320x240 range. Even I uploaded the running application from the EZtouch panel and saved it. Next time when I try to open it, the program showed the same message too. Does anyone experience the same problem? Is there a bug inside the program? My OS is Win 98, The panel is EZ-S6M-F 6 " mono 320x240.


  • adccommunitymod (AutomationDirect)

    Created Date: April 16,2002

    Created by: khfok

    Recently I upgraded my EZtouch editor software to 2.0. After I used it to create an application, next time when I try to reopen it, the program showed an error mesage saying that "Error S01_2: EZTouch editor detected that one or more objects ... outside the 320x240 resolution, ... " But my screen and all objects are fine and within the 320x240 range. Even I uploaded the running application from the EZtouch panel and saved it. Next time when I try to open it, the program showed the same message too.

    Does anyone experience the same problem? Is there a bug inside the program?

    My OS is Win 98, The panel is EZ-S6M-F 6 " mono 320x240.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: April 18,2002

    Created by: Tech Guy

    The problem you have experienced has been duplicated and reported to AVG. They are working to correect the problem in the next release of the software. The error is fairly easy to correct but hard to explain without writing a book. We will be glad to assist you in correcting the problem. Please contact ADC Tech Support at 770-844-4200.