adccommunitymod (AutomationDirect) asked a question.
EZTouch Numeric Limits
Created Date: February 15,2001
Created By: MLB
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Is there a way to put in v-memory for limits on the numeric entry objects? I would like to be able to set up a password protected screen to allow me to setup limits for my analog outputs. The scaling values as variables would be nice too. If not, that should be added as an option in subsequent versions. I suppose in the meantime I will have to use ladder logic to limit it.
Created Date: February 15,2001
Created by: MLB
Is there a way to put in v-memory for limits on the numeric entry objects? I would like to be able to set up a password protected screen to allow me to setup limits for my analog outputs. The scaling values as variables would be nice too. If not, that should be added as an option in subsequent versions. I suppose in the meantime I will have to use ladder logic to limit it.