TheColonel26 (Customer) asked a question.

When is a Raspberry Pi based Controller for the Productivity Line coming out?

When is a Raspberry Pi based Controller for the Productivity Line coming out?

 

Futher it needs Codesys drivers for the IO modules provided.


  • Tinker (Customer)

    I have no idea, but I wouldn't hold my breath.

    If I had a project that I wanted to do on Raspberry pi and use P1000 modules, I'd use a P1AM-100 as an interface. There are a number of ways the two could communicate, one could but the pi in a DIN rail case right nest to the P1AM and use SPI which might give maximum performance? Or use an asynchronous serial connection, or possibly the Ethernet shield,

  • ADC_AutomationControls_PE02 (AutomationDirect)

    We've sure noticed the enthusiastic response to our P1AM Arduino compatible line and we’re evaluating new products in the open source space. It’s difficult to provide timelines or commit to specific product features. Keep checking all the new products we launch each month!